FB#.BITS

Description

Specifies the number of BiSS sensor (position) bits for the BiSS encoder in use when used for linear motors. The required value for this parameter is provided by the feedback device manufacturer for the particular device being used.

Context

Only used for when FB#.MECHTYPE is linear and identified feedback is BiSS. See Feedback # View.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

position bits

Range

0 to 64

Default Value

26
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
FB1.BITS

3500h

06h

Unsigned16

-

-

Read/Write

No

FB2.BITS

3501h

06h

Unsigned16

-

-

Read/Write

No

FB3.BITS

3502h

06h

Unsigned16

-

-

Read/Write

No

FB4.BITS

3503h

06h

Unsigned16

-

-

Read/Write

No

FB5.BITS

3504h

06h

Unsigned16

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

FB1.BITS

30400

76C0

Unsigned16

Read/Write

-

FB2.BITS

30401

76C1

Unsigned16

Read/Write

-

FB3.BITS

30402

76C2

Unsigned16

Read/Write

-

FB4.BITS

30403

76C3

Unsigned16

Read/Write

-

FB5.BITS

30404

76C4

Unsigned16

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

FB1.BITS

30400

Unsigned16

Read/Write

-

FB2.BITS

30401

Unsigned16

Read/Write

-

FB3.BITS

30402

Unsigned16

Read/Write

-

FB4.BITS

30403

Unsigned16

Read/Write

-

FB5.BITS

30404

Unsigned16

Read/Write

-